The insert blocks can be used to press-in har-pakŪ
male connectors without any special top tool.
These blocks will be put into the connector manually or automatically (using
insertion removal station).
To press-in the connector no precise position is needed and can be done
by a simple flat rock die. This will accelerate the cycle time of the
press-in process dramatically.
Insert blocks are developed for use with a loadnest.